Dear Specialists,
My customer is evaluating UCC28019A and encountering the input current distortion.
I would be grateful if you could advise.
---
I am evaluating TI's PFC controller (UCC28019ADG4), but the input current waveform is distorted immediately after the load is turned on.
Could you please see attached excel file (UCC28014ADG4_Input_Current_Distortion_20200915).
The waveforms at 100V 60Hz and 264V 50Hz are shown in Figures 1 and 2, respectively.
At 100V, some distortion is seen in the first pulse, and then distortion is seen near zero cross.
At 200V, a large distortion is seen at about 8 pulses, and then distortion is seen near the zero cross.
Fig. 3 shows the circuit diagram.
Could you please let us know the cause and the solution.
UCC28019ADG4_Input_Current_Distortion_20200915.xlsx
About the shematic,
C15 is originally 1000pF, but to 4700pF for the noise suppression.
Current Sense Resistor (R54) is calculated 34mohm, but change to 27mohm because current limit is active earlier than expected.
Regarding circuit condition, could you please see the attached file (UCC28019A condition.xlsx)
---
I appreciate your great help in advance.
Best regards,
Shinichi