Other Parts Discussed in Thread: LM5141, LM5145
Hello team,
I'm testing a LM5141 EVM. It is in FPWM mode and output voltage is 5V. DC input is 8V.
When I increase the CC load to over 1.6A, the output voltage goes down to between 1.6V and 3.5V and jumping between this range, also the current can't be steady. While they never goes to 0.
This condition seems only happened when input voltage is below 16V, the output data looks well when I increase the Vinput.
Why is that happened?
Many thanks