Dear all.
Do you have a result of the load regulation of the following conditions?
Vin : 13.2V typ
Vout : 5V typ
Iout : 3A max
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all.
Do you have a result of the load regulation of the following conditions?
Vin : 13.2V typ
Vout : 5V typ
Iout : 3A max
Regards,
PAN-M
Hi Pan-M,
Thank you for posting. The design that you referred to just supports up to 2.5A rated current. This rating is for the entire VIN range and for sure the output current can be higher than 2.5V if you raise the input voltage. The output regulation is basically the feedback and it is not much affected by the input voltage as long as the SW peak current limit is not tripped. Therefore, you can basically see regulation at 3A to be almost the same level as at 2.5A.
Thanks,
Youhao Xi, Applications Engineering