Dear Specialists,
My customer is evaluating UCC28051 and has a question.
I would be grateful if you could advise.
---
We're in a final test before mass production and there is a output voltage drop in some board.
Could you please advise following questions.
---
(1) Tolerance of maximum output voltage of error amplifier
⇒ Is it "V comp high: 4.5V --5.5V" described in the data sheet P5 VCOMP high in VOLTAGE AMPLIFIER (VO_SNS) ?
(2) Related to Question(1),
When the error amplifier is saturated, the output will be the maximum COMP IN value of 3.8V, or will be the maximum output voltage of the error amplifier of 4.5V?
Which value should be used for 3.8V or 4.5V in the equation at datasheet of 7.3.6 Multiplier Block.
0.67 × VMULTIN × (VCOMP − 2.5 V)
(3) How much does the Multiplier gain constant (k) change with temperature?
Are 0.43Vmin and 0.87Vmax included temperature fluctuations?
---
I appreciate your great help in advance.
Best regards,
Shinichi