This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 7
Views: 59
Part Number: TPS54116-Q1
Hi Team
Regards,
Yuichi Shintomi
Hi Shintomi-san,
We will review and get back to you by 9/21.
Weidong
In reply to Weidong Zhu:
The schematic looks good, although some parameters (such as compensation) might need to be adjusted based on test results. I saw you have Webench simulation results already, but test results can have some difference.
PVIN has internal UVLO function, so the part will not turn on until PVIN reaches UVLO threshold (2.7V typical). In your application, please configure the sequence so that ENSW/ENLDO rise after PVIN reaches UVLO threshold.
Hi Weidong-san,
Thank you for your kind reply. Is the input method of the synchronous clock signal OK? In the case of synchronization, WEBENCH simulation rayon cannot be done, so it was carried out as a guide.
The power boot sequence is・ 12V input is input when the system starts up.・ Next, the FPGA that performs config and power control starts.・ TPS54116-Q1 starts at the third timing of the FPGA, which is responsible for the main functions.It starts in this order, so there is plenty of time for UVLO to work.
Regards,yuichi
In reply to user6057711:
The synchronous circuit looks good to me. I think you can test it out when you have the hardware.
For the power sequence, I assume 12V will be converted to 3.6V first, and then 3.6V will be supplied to TPS54116-Q1, and then FPGA will send out the control signals (ENSW/ENLDO). This sequence should be ok.
Thanks for the clarification, I don't see anything else wrong with the schematic.
Thank you very much.
Yuichi