Hi,
I am considering a Fly-Buck circuit using the LM5017.
The specifications are as follows.
I checked the TI documentation and found a transformer with model number 750314225 in the transformer selection guide, and I think this transformer can be used.
In addition, the reference design PMP9316 using this transformer is described in the material, but the material of PMP9316 is not published on TI's WEB.
Could you provide me with the PMP9316 schematic and bill of materials?
(specification)
VIN : 24V
OUT1 : 5V (insulation), 200mA
OUT2 : -5V (insulation), 200mA
Best regards,