Hi team,
LMR16030 is being used to go from vin 12-50V to output 8.25V with a max current of 2.5A and switching frequency around 900kHz. It is working fine however it is seen that the voltage across the BST cap is 7.5V which is higher than the 6.5V shown in absolute maximum.
Concern would be that this would have undesired long term effects for the integrated FET, do you know what could help address this higher voltage than expected?
Best regards,