Hi All,
Is there a buck-boost converter that can meet follow requirements:
- Input voltage form 4V to 12V
- Good dynamic output feature ,because input voltage will drop from 9V to 4V,
- Constant output current is about 4A.
- The required peripheral inductor height is less than 1.2mm
Is TPS55288 that best meet these requirements? Or is there any other product fits these well?
Thanks!