Hi, in the table 3 the Iout_max is calculated as 21mA using the formula Pmax/Vds_max =0.5/23 = 21mA.
In the datassheet of the M1 mosfet used in Figure 2 (CSD18541F5) the Vds_max is 60V and not 23V as stated in the table.
So the Iout_max would be 0.5/60=8.3mA
Is this correct?
Thanks