Other Parts Discussed in Thread: UCC24612
Ulrich:
I think I got it finally: the whole interplay of sws, hvg, ref, run , Ivsl limits , CS limits, output voltage slow start relationship.. etc. in an integrated manner: what I call the "zen" of it.
So I am going to get the circuit fitted with values from your details & I am sure it will RUN.
We have retested the xmfr(28:3:1) response, the upper GAN bias & the lower GaN bias, the secondary response/dc output with 10% load...& know that if PWML happens 1,2, 3,...5 times, etc.., will continue because of the setup.
Will keep the CS pulled up( with 60k to REF) until all aspects are checked out & we feel it is ok to go to 380V input.
Will report asap.
thnx so much!
robin