Hi team,
my customer is printing boards for prototyping now so i need to get this over to them by today.
they are using the TPS55340 in a boost configuration and are leveraging a past schematic.
their design requirements are as follows:
Input voltage min = 5.5V
Input voltage nom = 9
Input voltage max = 12V
output voltage = 28V
output load current = 0.8A
switching frequency = 630kHz.
max ambient temp = 60C
they have the following questions.
1. can we reduce the boost inductor (currently 10uH) down to 6.8uH? will the inductor specs provided in the link below suffice?
https://www.mouser.com/datasheet/2/597/xal4000-270751.pdf
2. can TI help identify if we can eliminate any passives (caps, resistors, inductors) from this design? (space is premium).
3. is the inductor (L405) necessary? it looks to be a pi filter.
Thanks,
Kevin