Hi,
We are using the BQ21040 with a Lithium Polymer cell that has a protection circuit already installed. I am currently testing performance at low voltage situations. Battery and charging circuit is connected to a constant 20mA load.
When the Lithium Polymer cell drops below 3V, it seems that its protection circuit disconnects (Open Circuit) for under voltage safety state. I try to charge with BQ21040 circuit by connecting external 5V but it seems that it cannnot charge battery any more. It cannot exit the safety state no matter how long the BQ21040 with external 5V circuit is connected.
To recharge my test battery, I disconnect from the test circuit and connect directly to a power supply (4.2V, current limit: 100mA), it seems to recharge no problem
Does the BQ21040 work well with existing protection circuits or must it connect directly to Lithium polymer tabs? I saw in the datasheet that the BQ21040 has a per-conditioning state, does this help get the protection circuit out of this safety state?
Thanks,