Other Parts Discussed in Thread: BQ24272
Hello,
We have encountered some issues with the BQ25601 VSYS output while there is no Battery and charging is enabled.
Our Load is a GSM modem, which draws burst current up to 1.5-2A.
While the charging is not enabled (CE PIN is Pulled Up) everything works fine, few mV drop on the VSYS output.
After we enable the charging (CE PIN grounded) we see the charging sequence, which tries to get the battery voltage to VREG (4.1V used), but while if a burst is encountered on the VSYS output the voltage drops below 3V which makes the GSM modem to stop working. It seems while VREG is applied for some reason there is current limit but we are not sure what happens. We have tested if we put a totally depleted battery it works fine, even if that battery probably is not capable of supplying 1.5-2A burst. We tried all kind of setting(REGITER setup), but nothing seemed to solve this issue, which is quite critical, because the battery is mounted by the distributor/client. Also the software is running on the GSM modem, so it's not like an external controller will disable the GSM modem till it checks if the battery is mounted or not.
Attaching a screenshot to be as clear as possible with my description.
Best regards,
Balazs