This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 4
Views: 70
Part Number: TPS55288
Dear TI support
Can you help check , Why I use TPS55288 PIN14( FB/INT) the function not implemented?
I use internal feedback, and external pull-up resistors, According to the function, it should be pulled down if there is a problem, but now OK work is also pulled down, please help to confirm, or point out how I need to use the abnormal function of FB/INT, I need to use this PIN to judge the working status。
Thanks !
Dear Sir,
Could you please share the schematic with us, does the INT pin pulled high? Please refer to the TPS55288EVM board, there's a 100k ohm resistor pull high to a 5V VCC.
Best Regards,Helen
Boost DC/DC Solution
In reply to Helen chen:
Dear helen:
The circuit diagram is as follows, we have a pull-up resistor, and the software is set to internal FB function.
In reply to user4720651:
I checked on the EVM board, the INT function is good.
Please check the setting in your I2C, is it well set? Please compare with below picture.