Could you offer the thermal derating information @Vout=3.3V? The curve diagram is Ambient temp versus Output Current.
application: Encoder for Motor drive
Working Ambient Temp: 105degree
Regards
Brian W
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you offer the thermal derating information @Vout=3.3V? The curve diagram is Ambient temp versus Output Current.
application: Encoder for Motor drive
Working Ambient Temp: 105degree
Regards
Brian W
Hi Brian,
I'm unsure which curve diagram you are referring to. The important consideration here is to not exceed abs max temperature. The Electrical Characteristics table was generated for temperatures up to +125C, so if you wish to stay within that range then you have +20C rise to work with, otherwise you have +45C rise to stay within the abs max range of +150C. This assumes an ambient temperature of 105C.
Next you need to determine your junction to ambient thermal resistance for your board. For the 3 values in the datasheet, you have:
DRB: 379mW (20C rise), 852mW (45C rise)
DCQ: 168.5mW (20C rise), 379mW (45C rise)
DBV: 90mW (20C rise), 202.8mW (45C rise)
Now you just need to find the watts dissipated: (Vin - Vout) * Iout = Pdiss
Thanks,
- Stephen
Please offer thermal derating for below package. thanks.
TPS73633MDBVREP
TPS73601DBVR
Thanks Stephen.
May I get one more curve for TLV73601DRBR/SON package? thanks.
Regards
Brian W