Dear Ti team,
I have a new design using LM5145 and the input is 28V, output is 5V 10A and the switching frequency set to 130KHz.
But, I have to check the switching frequency using oscilloscope under no load and full load. I find that the witching frequency of the LM5145 drops to 68kHz after turned on the step down converter about 5 minutes. This state can only be reset by completely resetting the converter (turn off power longer than 5 seconds). This problem is it related to bode plot?
Please find attached for my calculation. Would you please help to review?
BR
Kevin
LM5145 Wide Vin Synchronous Buck Controller Quickstart Calculator r12-7.zip