Hi,
my customer is using BQ25790 with Two ACFETs-RBFETs.
When they enable OTG, they will write EN_ACDRV1 = 1 to enable output on VIN1.
Then if they exit OTG, besides disable OTG, do they need to reconfigure EN_ACDRV1=0?
Then if another power source is attached to VIN1, the device will automatically set EN_ACDRV1=1 without host control, right?