hi. The LDO output is set to 1.58V and operates as a strong pull up voltage, with 40Ohm resistor to point A
I have two questions:
- At some moment the voltage in point A might be 2V because of other device connected to this point. does the LOD is capable of sinking a current of 10mA? if not can I change the feedback resistor so the current will flow through them?
- When point A is disconnected (no current is flowing) the output voltage is the same as the input voltage and stabilizes on the desired value only when the current is approximately 4mA