This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPS55288: Default output voltage

Mastermind 8005 points

Replies: 1

Views: 26

Part Number: TPS55288

Dear team,

The output voltage of the default of this device is;
Vout = Vref x (1+ INITFB)
Vout = 0.282 x (1 + 0.0564) = 0.298V
Is this correct?

And, is there no change in RTM of TPS552882?

Regards,
PAN-M

  • Dear Sir,

    The default output voltage of is 5V for TPS55288. Vo_default=0.2822/0.0564=5V.

    For the TPS552882,Vref=1.2V.

    Best Regards,
    Helen

    Boost DC/DC Solution

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.