Part Number: BQ27441EVM-G1A
Hi,
I'm using BQ27441-G1A for gauging VARTA EasyPack PLUS.
In our case, we have to minimize as much as possible the DSG Current threshold and Quit Current
Following the datasheet(SLUUAC9A), the maximum value of the Dsg current threshold is 2000 and the maximum value of quit current is 1000
knowing that the design capacity of the used battery is 5200 mAh and according to the datasheet,
the minimum discharge current is 26mA, and the minimum Quit current is 52 mA.
But if I understand, the relaxation state is an intermediate state between charge and discharge states,
so the discharge current should be greater than the Quit current so if we want to choose the Quit current value as 52 mA(the minimum value),
The discharge current should be at least 57 mA. Do you confirm that?
If yes, is there any way to ignore the relaxation state? (per example by setting quit current register at 0)
Best Regards,
Mehdi