Part Number: BQ24600
I could use some help diagnosing operation of a BQ24600 battery charger IC on our prototype circuit. We are using it to charge a single-cell Li-Ion battery. Fully charged set point voltage = 4.2V. Charge current is set to 0.5A. Below I included the schematic for the circuit we have on our PCB.
This circuit was working OK for a few days, but for the last few weeks I get the 1/2 Hz error pulse on the STAT output pin almost immediately after powering up the PCB. I tried 2 different cells, one measured about 3.18V and the other 4.12V. The charger does the same thing regardless of which battery is connected, even if I manually discharge the 4.12V down to 3.95V, and it also does the same thing if I power up with no battery connected. The STAT output pulses BEFORE I even drive the CE input high.
I am looking through the data sheet but I can't determine the exact problem. I measure 3.3V on Vref and about 1.65V on Ts, so I do not think the RTD is too warm. The voltage on the Vcc pin measures 4.8V. Can you offer any suggestion as to what might cause this? I am thinking the key might be that it pulses the output immediately after powerup, before I have CE driven high.
Thank you
John