We are utilizing the LMR16006Y in a design to regulate a supply from 20-44V down to 15V.
Application load current is 118mA. Output capacitance is 41uF.
When power is first applied, the regulator switches at 172kHz-500kHz instead of 2100kHz. In addition, the output reaches steady state at approximately 3.16V instead of the designed 15V.
Rapidly cycling power to the regulator results in proper operation (2100kHz switching with ~14.9Vrms output).
The issue returns after removing power for ~20 seconds prior to re-applying power.
Attached are scope captures for the regulator turning on. For the following two images channel 1 is Vin (24V SLA Battery), channel 2 is the output voltage, and channel 3 is the SHDNn pin.
For the following three images channel 1 is SW pin, channel 2 is the output voltage, and channel 3 is the SHDNn pin.
Is our input supply ramping too slowly for the LMR16006 to turn on correctly?
Are there suggestions on where to look to resolve this?
Thank you.
Please note: adding hardware to forcibly power cycle the regulator during boot is a band-aid solution that we will only pursue as a last resort.