Hi,
I am using a TPS23881 on my board (see attached schematic). It has 8 channels and I want to configure it so as to handle 6 ports :
channel 1 for port 1 (30W PoE+)
channel 2 for port 2 (30W PoE+)
channels 3&4 for port 3 (90W HiPoE)
channels 5&6 for port 4 (90W HiPoE)
channel 7 for port 5 (30W PoE+)
channel 8 for port 6 (30W PoE+)
I have started my board and every channel seems to work fine.
Now I need to program all the registers in order to combine channels 3&4 and channels 5&6. How should I configure the TPS ?
About the Power Allocation settings (reg 0x29), is it the maximum power configuration for all the port ?
I need full power on ports 3 & 4 (4-pair 90W). What will happen for the other ports (2-pair 30W) ?
I think I have to program 0x29 Reg with 4-pair 90W configuration. Is that right ?
Best Regards
Stephane