This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28711: 3-phase input dc dc converter part suggestion required

Part Number: UCC28711
Other Parts Discussed in Thread: UCC28700

I need a part advice for my dc-dc converter design idea, which is rectified from 3-phase 120-400VAC(phase to phase) - 50 Hz. The output should be 24VDC/2.5A max. Output regulation does not need to be tight and there is no transient overload is required. I have 3 parts in my mind: UCC28711, UCC28700 and UCC2863X. Which one is easier to use and best suited my requirements? Thanks.