Hello,
I am looking at how to connect PG pin of LMR36520. I do not need to use this function.
In the datasheet (SNVSBF0B –SEPTEMBER 2019–REVISED APRIL 2020) it is written :
- page 4, Chapter 6 Pin configuration and Functions: "Can be left open when not used."
- page 10, chapter 8.3.1 Power-Good Flag Output: "If this function is not needed, the PG pin must be grounded."
Should I leave it open or connect to ground?
Best regards,
Louis