I designed 4-layer PCB with LM5143-Q1.
Configuration:
Vin = 24V
Vout1 = 3.3V, Iout1 = 7A
Vout2 = 5V, Iout2 = 10A
My question is: It is possible to provide correct functionality only on 4L PCB instead of 6L PCB? In my PCB desing tracks coming from current sense resistors is routed under the power MOSFETs. In evaluation board these tracks are routed in separated layer back of the power MOSFETs. Do I have to use a 6L design instead of a 4L design?
Thank you.
Best regards.
Samuel