Bq24070, the charging current I set is 900mA, please refer to the circuit diagram, but the actual circuit reaches 2A charging current in the charging state, STAT1 stat2 is displayed in the fast charging state, R45 = 1.2k Ω is used to set the charging current, please help to analyze the problem?