Hi Team,
Hope you're well.
Start time for my design is 3ms when the output is 350mA, but the start time becomes 40ms when it works in analog dimming mode with a lower output of 75mA.
Topology: buck-boost
Input: 12V / 24V
General mode: Io=350mA, ts=3ms, V-IADJ>2.5V
Analog dimming mode: Io=75mA, ts=40ms, V-IADJ=511mV, no any other changes with general mode.
What I want is the start time can also be 3ms when it works in analog dimming mode. Could you please help to analyze this issue ? What might I have a try ? Thanks a lot.