Other Parts Discussed in Thread: LM73606
Hi, TI expert.
A customer company constructed a circuit using the LM73606-Q1, and I have a few questions regarding it.
-INPUT: 5V, OUTPUT 4V
(Questions)
1. Fsw: Use 500KHz (Is Fsw suitable?)
2. Is the power inductor applied to the circuit suitable?
3. Is the Input CAP / Output CAP applied to the circuit suitable?
4. Are there any other parts to be added or modified?
Please confirm and reply.
Please tell us if you have any further questions. Thank you.