Other Parts Discussed in Thread: TPS61500
Considering the TPS61165 *SEPIC* configuration, what are the formulas for calculating power dissipation and Vout max & min?
The input voltage is between 12.5V and 13.6V, the output current is 350mA, and the ambient temp is 40°C. What is the maximum and minimum output voltages to which we can design the circuit?
Thank you!