Other Parts Discussed in Thread: BQ24073, BQ25606, STRIKE
Dear Sir.
Could you help me with the BQ25616 and BQ24073 ?
I designed my charger with BQ25616, it works well.
But to save the system cost and the space, I am checking the circuit again.
Q1:
I designed an OVP circuit for the BQ25616 and tested, Is it ok if I remove the OVP circuit for the BQ25616 ?
The input voltage of bQ25616 is max 16V.
I need to reduce BOM and space.
I am using a 1A adaptor.
The battery charge current is 1C and capacity of it is 850mA.
When the battery was fully discharged, it needs 850mA for charge at initial state, and to operate the system, it also needs max 800mA.
The adaptor current is lower than 1.65A(850 + 800mA).
After device works with 800mA, it entered into idle mode , the current consumption is 20mA in the idle mode.
Q2:
In this case, does the BQ25616 reduce the charge current to supply sufficient current to the system ?
and if the device enter into the idle mode, the BQ25616 supply 850mA of charge current to the battery again ?
Q3:
In this case, does the BQ24973 reduce the charge current to supply sufficient current to the system ?
and if the device enter into the idle mode, the BQ24973 supply 850mA of charge current to the battery again ?
Best Regards,Yoon.