Part Number: TPS63031
Hello.
1. Do you need to connect PS/SYNC to ground to enable power save mode?
2. DC/DC is always connected to the touch sensor, which consumes 59uA. Does EN need to be connected to VIN in order to put the DC/DC to operation, or can it remain connected as it is now, across a capacitor to ground?
3. Do I need to change the VINA connection?
4. What is the minimum DC/DC current consumption I should have with the switch off, 35uA, or is it some other state other than Quiescent current (Shutdown 0.9uA)?
5. Is it possible to input DC / DC into Shutdown current when I connect, so that the touch switch continues to work and can turn on all peripherals?
Connection diagram is attached.