This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: BQ25606 ISSUE

Part Number: BQ25606

3. The ICHG resistance is changed into the battery indicator light with 470 resistance of 3.1V, and the indicator 1a current on the 5V side of the test with the battery of 3.43.8V is normal. The current is set to 2.5a, and the battery voltage is 3.4V now.When the battery is not discharged under normal conditions, the output is normal 4.2V, and when the load is added, it does not work.。