This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 65
Part Number: UCC5304
Do you have a version of UCC5304 with an ENABLE pin?
Best regards,
Don Dapkus
Gate Driver Applications
Dallas, TX USA
We have an excellent training series that can help answer all your questions about our gate drivers. It is indexed so you can jump right to the section you want! You can find it here. A second series focused 100% on Isolated Gate drivers may be found here.
We also provide models for our gate drivers to accelerate your time to market. You can find them in the Product Folders under the "Design and development" tab:
There are two options here:
First, you could add an external logic gate to accomplish this:
Second, you could use UCC5350 instead. This does not require the use of the AND gate. See this FAQ for more information.
If you have further questions about this topic, or any other topic, please post a new/related question and our team will be happy to help you.