Other Parts Discussed in Thread: LM61440, LM61460
Hello,
I want to regulate the output voltage of LMR33640ADDA with a control voltage.
So I modified the schematic diagramm (color green).
The control voltage is between 0V to 5V.
And the output voltage should be between 15V to 0V.
The Output Current depends on the load and is max. 3A.
Could you please take a look if these modification are a violation of the design rules of LMR33640ADDA?
Thanks,
Alen