Part Number: LM5164
Hi there,
this is probably more of a general question regarding switching power supplies... or maybe it is indeed part specific. Not sure ;)
I'm using the LM5164 for many of my boards where I need buck converters to step down from 48-80V to 5V.
In order to be able to program the micocontroller, some boards have an ISP oder debug connector on them.
Thus, a USB programmer can also directly supply the 5V rail through the ISP connector.
Now I was wondering... do I have to protect the LM5164 against "reverse voltage" by placing a diode right behind it?
Imagine the 48V main supply was disconnected and the LM5164 was inactive, but 5V rail was supplied via ISP...
Looking forward to your thoughts! Thanks ahead.