This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33610: Inductor Value

Part Number: LMR33610

Good Afternoon,

 

I'm looking to choose an Inductor to be used with this part. I'm currently looking at the A variant (400kHz fsw).

Using WBench, an inductor of 15uH has been chosen; but using the formula in the datasheet it recommends a minimum of 220uH (roughly).

 

Using 0.3 for the constant k. Range of the input is between 10V and 16.8V; 16.8V used in the formula. The output being 3V3 @ 100mA.

Which value would you recommend using?

 

values summarised as:

Vin = 16.8V

Vout = 3.3V

K = 0.3

Fsw = 400kHz

Imax = 0.1A

Many Thanks