Datasheet is described L and Cout recommend value, attached below.
Can L and Cout value exceed recommend range, no problem? (For example, L: 2.2μH~ and Cout: 200μF~)
【Background】
・I simulating TPS63802 with Vin: 3.3V~4.5V, Vout: 5V, Iout: 1.8A, FPWM, on Webench tool.
But, when simulating Load transient and Input transient, peak current became large and reach current limit(4A_min, 5A_typ).
・I trying to adjustment good peak current.
When increase L and Cout value became a little decrease peak current, but transient voltage getting worse.
・I guess that datasheet recommend value is the condition of stable with TPS63802's internal compensation specification. (is it correct?)
If my guess is not correct, I will consider to change L and Cout value much larger than recommend value for decrease peak current.
If there the other idea for good transient specification, please let me know together.
Best regards,
Satoshi