Other Parts Discussed in Thread: LM61495-Q1, LM5176-Q1
hi,
i'm planning a card to an automotive purpose but not a critical system - can be called infotainment....
i can't understand if i must take only AEC-Q-XXX compliance parts ot i can use usual parts. it is a problem in all the card i'm planning and it is very difficult to find these parts.
for instance i'm now looking for dc/dc power module 12V to 5V/7A and i can't find anything like that, especially with the AEC-Q-XXX compliance.
does anyone can advise me?
br