Other Parts Discussed in Thread: BQ76952, BQ34Z100, BQSTUDIO
Hello;
My client's BMS uses the new bq76952 Monitor/Protector and the bq34z100 fuel gauge. Both measure the sense resistor. Both are calibrated for board offset and CC gain/offset. However, while the 952 correctly applies this board offset to its reported current measurement, the 34z100 appears not to do so. After calibration, the 76952 reports 0 to 1mA of current when there's no current flowing, but the 34z100 reports -49mA, both before and after calibration.
Both the host u/C's calibration routine and bqStudio's calibration procedures produce the same results. After board offset calibration, the gauge should report the same as the 952, or very close to 0mA.
Since I cannot find any errata sheet for the gauge, this would appear an issue.
What could cause this? Or what am I missing?