Hi Sir,
could help reply the following question? thanks for your great support.
MCU MSP430F5234IRGZR can be omitted. (Yes or No)?
If no, whether to add SRAM on external?
We use TPS23881 need add the I2C SRAM component.
Q1. Because of the datasheet, TPS23881 SRAM 16K (Does it include the code size?)
PS1: how much space does the code occupy?
PS2: Can we plug-in Flash or SRAM to achieve Programmable and application? (Do you have an actual SRAM application data or design guide?)
PS3: If need use external SRAM, can you provide the relevant information? (Which brand and specification is the size of the SRAM used?)
Q2. SDAI and SDAO can be connected with non-Isolation. (Can you provide us with a reference design link?)