Other Parts Discussed in Thread: BQ34Z100, GPCCHEM, BQ34110
Dear TI Support Team,
We have an application that uses the bq34z100-G1 fuel gauge.
We have completed a successful learning cycle and have created a golden image from it.
When we program the golden image .srec file to new packs, enable IT, everything looks okay.
However, when the packs get into the field, inaccurate fuel gauging has being reported.
We have seen the pack get to 100% prior to reaching FC. There are times when the pack will hang at 100% before counting down on discharge to 99%..98% and so on.
This will then lead to the pack suddenly dropping from 30-20% down to 0% at the end of discharge.
It seems as though by a 4th or 5th cycle, the fuel gauge reports more accurately.
Does this mean that each pack will need to undergo it's own learning cycle?
Appreciate any feedback.
Best Regards,
Kevin