Replies: 10
Views: 141
Part Number: TPS25924
Dear Specialists,
My customer is considering TPS259241 in parallel referring to the application note(slva836).
They has a question about the layout.
I would be grateful if you could advise.
---
When TPS26400PEPR is connected in parallel, UVLO, OVP, ILIM resistor and dV/dT capacitor) are used in common.
Is there a recommendation for where to put the parts?
Which device side should those parts be placed on?
Are these parts on one device side?
Are these placed in the middle of each device?
Please let me know if there are any other suggestion regarding pattern design.
I appreciate your great help in advance.
Best regards,
Shinichi
Hi Shinichi,
Can I know the max load current in customer application ?
SLVA836 is an old Application Note when we do not have high current eFuse devices in our portfolio. Now, we have TPS25982 which can be used for 14.7 A current limit. TPS25982 also has more advanced features including programable no. of retries, Programmable timer duration to allow transient load currents.
The overall solution size and cost would be less for TPS25982 when compared to the parallel solution with TPS25924.
Regards,
Praveen
------------------------------------------------------------------------------------------------------------------------------
Please click "This resolved my issue" button if this post answers your question.
To find latest information on efuse and Hotswap, visit www.ti.com/PowerSwitch
In reply to Praveen GD:
Hi Praveen,
Thank you for your reply.
I'm sorry for the lack of exlpanation.
In this case, the customer is considering TPS26400 in parellel and referring to SLVA836.
They'd like to know where to place the component regarding UVLO, OVP, ILIM resistor and dV/dT capacitor.
Could you please advise.
I appreciate your great help.
In reply to Shinichi Inoue:
Thanks for the detailed explanation.
I will loop in the right Apps Engineer to answer your question on TPS26400.
I'm looking forward to waiting the answer.
I appreciate your great help and patience.
The parallel configuration of TPS26400 will be similar to TPS2660.
Please refer attachment in https://e2e.ti.com/support/power-management/f/196/t/735218 for the TPS2660 parallel configuration and test results.
Regards, Rakesh
--------------------------------------------------------------------------------------------------------
To find the latest information on Power Switches, Visit www.ti.com/powerswitch
In reply to Rakesh:
Hi Rakesh,
Thank you for your reply and sending helpful information.
I have some question, could you please advise.
Accordig to the document, UVLO, ILIM resistor and dV/dT capacitors are set separately.
On the other hand, In SLVA836, these components are used in common.
(1) Could you please let me know pros and cons.
(2) When UVLO, ILIM resistor and dV / dT capacitors are set for each device,
the component variation and circuit characteristics will differ for each device.
Does this have a bad effect?
(3) When the parts are used in common,
the distance between the device and the parts becomes long.
The circuit characteristics are different because the distance between the component and the device is not constant.
Is there a negative effect?
I appreciate your great help and cooperation.
Common UVLO, OVP resistive ladder can be used just like SLVA836
Accordig to the document, dV/dT capacitor C2 is common
ILIM resistor has to be separate for TPS2640x and TPS2660x devices. This is the need as per PS2640x and TPS2660x device architecture.
The components can be placed in equidistant from the eFuse devices.
Best regards, Rakesh
Thank you for your reply and advise.
There are some question about when UVLO, OVP resistor and dV/dT capacitor use in common.
The distance between the component(resistor and capacitor) and the each device.
In this case, timing may be different.
Is there a problem.
Or it should be equal.
Please ensure both devices have uniform ground reference in layout. As these are voltage inputs to the device, there would not be any problem.
I understand it should be careful about GND potential.
I'll share your suggestion with the customer.