This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 60
Part Number: TPS6521815
Hi,
I would like to implement conformal coating on my product.
Is it possible on TPS6521815?
Hello,
Are you planning to implement the conformal coating below the device package as well or only around the PMIC?
If you are planning to put the coating under the device, it might affect the solder reliability of the device over the life time (depends on application conditions) and it may be difficult for us to provide the confirmation on this. However, I have forwarded your request to this device expert and he may have more information on this.
Regards,
Murthy
Find the right power solution for your processor or FPGA. Visit www.ti.com/SoCPower today!
In reply to Krishnamurthy Hegde:
TAKA,
My response is the same as my colleague, Murthy :-)
Thanks & Best Regards,
Brian
>Conformal coating around the PMIC, after assembly: There is no anticipated issue with this approach
Here's what I want to do this time.I understood this.
Thank you.