Hi Dear Support!
I'm trying to run the device from WEBENCH designer, here's the link:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dear Support!
I'm trying to run the device from WEBENCH designer, here's the link:
Oskar,
Thanks for sending along and your interest in TI here. I've assigned to an applications engineer to assist. Please expect a reply by end of day Monday Dallas time.
Regards,
John
Hi,
Do you mean you tested your circuit on bench after you built your board?
Hi,
I have built the circuit from the link and now I'm testing it. Output voltage at 31V Vin od about 27 V and decreasing with any load, like for 100mA output current it is 17.3 V. Shapes od signals Vds and Vgs are fine, but i noticed the %DC are always at max lvl (about 47-49% DC) for both IC's outputs
From:
Vct = 1,05*Vin = 1,05* 50 = 52,5 (53)
N = Vct/Vout = 53/24 = 2,208 and that's my transformer turn ratio. Did I calculate it correct?
Hi,
You need to add the duty cycle value into the calculation.
Let’s use the Datasheet page 12 circuit diagram.
Np1/Ns1 = (Vin / (Vout+Vf) x duty x 2
Fill in Vin with your minimum input voltage, Vout your maximum output voltage, Vf your secondary diode voltage 1V, duty < 48% suggest initial 40 %.
For example, Vin min = 30 V, Vout = 24 V, duty = 40%, then Np1/Np2 = 30 x 80% / (24+1) = 0.96.