Hey team,
A customer is having an issue with 3 prototypes with the following targets / specs:
OVP = 67 V
UVLO = 35 V
R1 = 200k, R2 = 3.3k, and R3 = 6.2k
They foudn that UVLO is working properly with 35V off and 37V on, but OVP is occurring around 57V. Any feedback on the design here?
Vin max = 67Vdc
Vin min = 35Vdc
Vin nominal = 54Vdc
I pointed out that R1 in the typical application was 100k, but the customer was trying to minimize quiescent current over UVLO/OVP accuracy.
When I ran the calculation for R2 I found it should be speced at 6.4kOhm unless I missed a factor of 2 somewhere? Just wanted some feedback on this