Hi, May i know the length of the lead as attach below?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, based on the drawing show that part of the lead will be under the boy. 1.2/0.8 is the length from the lead toe until the edge of the body only. i like to confirm the total full lead length including the lead length under the body if possible.
Hi, pg 60 land pattern shows a maximum size of 1.5. I do not currently have the information for the section under the body but it is not critical to the land pattern.
The best I can do is measure a device but i cannot give you a max or min deviation. Is that acceptable?