Hi,
I am trying to use the TPS55288 to power my system (4V) with two different power sources: 20V (Solar Panel) or 3.3V (Battery). I am powering the VCC from an external 5V but I only see 0.6V at the output.
I am using internal feedback, no output current limit (ISP, ISN, and VOUT connect all together), MODE = 75kΩ. I was expecting initially to get 5V base on the default value of the registers Reference Voltage and Feedback Selection.
I will highly appreciate it if you could help me with the debugging of my design. I have the files from my design available in case they can be useful.
Kind regards,