This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62095: Abnormal output

Part Number: TLV62095
Other Parts Discussed in Thread: TPS62868

Hi

Q10 gate pin is connected to 3.3V, output 0.9V => normal

1. The Q10 gate pin is connected to an empty connection and the output is about 0.2V but the output becomes 1.05V => abnormal

2. When Q10 gate pin is connected to GND, output becomes 3.3V => abnormal

Q10 Replace 2n7002 and it is normal

FDV301N-D.PDF