t Number: UCD90160A
HI
UCD90160A has been used on our E7-2 line card, the schematics and configuration firmware of UCD90160A are attached. We’ve met an issue, 3V3 is disappeared, but all the other rails are still good. And looked at the signals on the board, UCD90160A itself power supply is good, and all the other power rails are good, and UCD90160A drove a low 3V3 enable signal (3V3_PS_EN ) to 3V3 converter, that means UCD90160A disable the 3V3 converter. The questions are:
1. Since 3V3 is low, why UCD90160A hasn’t re-sequenced the power rails?
2. What’s the possible reasons that UCD90160A disable 3V3 converter, the 3V3 dependency, 0V95 and 0V9 are fine. and 2V5 and 1V8 have the same dependency as 3V3, and both 2V5 and 1V8 are good on the card.
Some signals are tested, and highlighted below:
|
|
DC(V) tested with digital multimeter in DC mode |
AC(mV)tested with digital multimeter in AC mode |
Notes |
|
3V3 |
1.12 |
20 |
Low voltage |
|
3V3_PS_EN |
0 |
|
Why PMON shut down 3V3 only, have tested two test point, one is close to PMON, the other is on 3V3 Converter ZL6106, both are low |
|
PWR_GD_3V3 |
0 |
|
Low indicates 3V3 is not good |
|
3V3_PM |
3.3 |
10 |
PMON power supply is good |
|
PMON_3V3 |
0.71 |
|
Since 3V3 is 1.12V, PMON_3V3 is 0.7V |
|
PMON_PG_LED_N |
3.3 |
|
High means, PMON power good LED is off -DS11 is off |
|
PMON_PORST_N |
0 |
|
Since 3V3 is low, that generates a low PMON_PORST_N--DS13 is on in RED |
|
PMON_SYS_FPGA_GRST_N |
0 |
|
Since 3V3 is low, that generates a low PMON_SYS_FPGA_GRST_N |
|
FRC_CPU_PORST_N |
1.8 |
|
This is good, system FPGA hasn't driven CPU power on reset |
|
All the other power rails |
Good |
|
|
Thanks
Frank